How to make the highlighting of associated edges of PMI easier to see?

2024-03-31T18:03:44Z

Summary


Details

It’s difficult to view the highlighting associated edges of a PMI when the PMI is selected.

How could I make them visible better?

Solution

The default color of highlighting could be changed by the following setting in customer defaults.


Also, "Show Width" can be  turned ON in the below preferences.



Still if the width is not enough, the solid body line width from the below preferences can be changed. Please note that this will change all the edges of the solid bodies.


KB Article ID# PL8784577

Contents

SummaryDetails

Associated Components