Solid Edge Solid Edge Update or Maintenance Pack Silent Uninstall Command Lines FAQ Master

2024-08-15T11:04:01Z
SETUP

Summary


Details

Administrators of Solid Edge installations are sometimes requested to uninstall a specific Maintenance Pack or Update of Solid Edge.

This can be challenging if they have to do this for more than only one or two workstations. In such cases, it is often helpful if this can be done by script over a network connection on the workstation instead of having to do it manually on-site.

Therefore, a command line is required, which can be implemented in a script, to silently uninstall the Maintenance Pack or Update from Solid Edge.

Such a command line is unique for each separate Solid Edge Maintenance Pack or Update.

Are these specific command lines provided somewhere?

Solution

Please choose the link related to the Solid Edge release of interest.

KB Article ID# PL8784186

Contents

SummaryDetails

Associated Components

SETUP: INSTALL