Unable to generate shell on spheroid shape

2024-03-26T05:16:55Z

Summary


Details

When trying to generate a shell after creating a solid shape using Revolve command for an ellipse created with a sketch, an alert saying "Preview could not be completed." is output. In addition, even if running the command with "Preview" turned OFF, the error "Cannot apply shell." is output and the shell cannot be generated.

Reproduced Steps:

1. Create a sketch section for rotation


2. Perform Revolve ( Start Angle = 0, End Angle = 180)


3. Perform Shell with Open option


Performing the command with Preview = OFF:


Solution

This behavior is due to NX problem and will be fixed in NX 2406.

Workaround : create the solid with End Angle = 360 > generate Shell with “Closed” > using Trim Body, Split Body or etc.

Notes

The problem occurs only when creating a revolve solid from an ellipse section at the angle = 0 - 180.

**Please refer to PL8783209 for Japanese article.

Release Versions
  • NX V1946.3700
  • NX - DESIGN V1946.3700
Platforms
  • Windows x64 10
  • Windows x64 11

KB Article ID# PL8783210

Contents

SummaryDetails

Associated Components