After creating Coordinate Note(Legacy), when I try to create it again, the strings such as "X", "Y" and "Z" that are entered as initial values in the dialog are cleared, and the input field becomes empty.
Reproduced Steps:
1. Create Coordinate Note(Legacy)
2. Again try to create it
This behavior is due to NX problem. There are existing PRs.
Workaround: Press Reset button in the dialog or enter “X=“ manually in the field
NotesIt occurs in NX 2306 and NX 2312.
**Please refer to PL8783205 for Japanese article.