Unable to suppress/unsuppress PMI from Details panel

2024-03-26T01:44:01Z

Summary


Details

A feature's suppression parameter is displayed in the Details panel, allowing you to control suppression/unsuppression. However, PMI does not display that parameter. Although it's possible to control that from the expression command, it's very time-consuming to perform the expression command each time. Is it possible to perform same operation as Feature?

Reproduced Steps:

1. Created PMI

2. Menu > PMI > Suppress PMI Objects


3. Part Navigator > Detail panel


Solution

This behavior is working as designed.

Workaround : Suppress/unsuppress PMI from the user expression node in Part Navigator.

- Menu > Tools > Utilities > Expression > select the created suppression expression > Show in Part Navigator


*** Appears in User Expressions node and can be controlled to suppress/unsuppress.


Notes

***英語記事につきましては、PL8783158をご参照ください。

Release Versions
  • NX V2212
  • NX - PMI V2212
  • NX - DESIGN V2212
Platforms
  • Windows x64 10
  • Windows x64 11

KB Article ID# PL8783159

Contents

SummaryDetails

Associated Components