NX Customer Defaults option "PMI reference CSYS " not found

2024-03-26T01:19:21Z
NX for Design

Summary


Details

The following item in "New PMI customer default options" described in "Feature template PMI enhancements" in "What's new in NX 2212" is not found in Customer Defaults.

1. "What's new in NX 2212" > Feature template PMI enhancements

New PMI customer default options

・PMI reference CSYS uses a CSYS that allows for better placement and orientation of PMI annotation planes on instantiation from a template.

https://docs.sw.siemens.com/en-US/doc/209349590/PL20220512394070742.whatsnew/xid2131129

2. File > Utilities > Customer Defaults...

Solution

This is due to documentation issue.

There is no Customer Default setting to make use of this function. It can be used without any settings.


Notes

**Please refer to PL8783148 for Japanese article.

Release Versions
  • NX V2212.5000
  • NX - PMI V2212.5000
Platforms
  • Windows x64 10
  • Windows x64 11

KB Article ID# PL8783149

Contents

SummaryDetails

Associated Components

PMI