"Label as Modeling Component" is not available

2024-03-26T01:16:12Z

Summary


Details

Instructions on how to configure Early Access Feature to enable this feature are described in "What's new in NX 2312". There it says to set "Assemblies_ASMBAS052" = ON, but when I check it, I can't find it.

Reproduced Steps:

1. What's new in NX 2312 > Design (CAD) > Assemblies > Synchronous assemblies

https://docs.sw.siemens.com/en-US/doc/209349590/PL20230425446868577.whatsnew/xid2250502

ー> It’s written as ”Set this early access feature to On in the Early Access Feature dialog box: Assemblies_ASMBAS052. “.


2. File > Utilities > Early Access Feature

->”Assemblies_ASMBAS052” does not exist.

Solution

This is due to documentation issue. This will be removed from “What’s new in NX 2312”.

In addition, correctly, by setting "Enable shape change with component positioning" = ON, "Label as Modeling Component" command will be available.



Notes

Refer to Documentation “Synchronous assemblies”:

***The correct information is posted here.

https://docs.sw.siemens.com/ja-JP/doc/209349590/PL20230425446868577.assemblies/xid2274166


**Please refer to PL8783144 for Japanese article.

Release Versions
  • NX V2312.4000
  • NX - DESIGN V2312.4000
Platforms
  • Windows x64 10
  • Windows x64 11

KB Article ID# PL8783146

Contents

SummaryDetails

Associated Components