Density value is shown as zero in NX 2306

2024-05-23T05:57:04Z

Summary


Details

Density value is shown as zero in NX 2306

Steps to Duplicate

1. Create a Block Feature

2. Analysis -> Measure

Select the Block

Density value is shown as zero.

Solution

NX is not truncating the value in Measure – just rounding as NX is following the “Decimal Places” setting in the UI Preferences.

Changing this display preference to ten decimal places instead of the default four, like below:


Now perform Analysis -> Measure


KB Article ID# PL8782869

Contents

SummaryDetails

Associated Components