NX How to modify precision in mass properties columns.

2024-03-21T07:00:00Z
NX for Design

Summary


Details

sometimes it is necessary to adjust the number of comma digits in the ANT.

Solution

The precision in mass properties columns in the ANT (and mass property panels) can be adjust by modify the decimal digits via the User Interface Preferences in the Dialog and Precision area.

Notes

The Navigator ( ANT) code picks up the decimal places from the UI Preference dialog.

We can change this to upto 11 (max)


Example: decimal places 2


Example: decimal places 6


KB Article ID# PL8782289

Contents

SummaryDetails

Associated Components

NX Legacy Documentation