Solid Edge Solid Edge 2024 Update 4 Announcement

2024-03-18T15:00:44Z
L10N PROFILE/SKETCH GENERATIVE_DSGN SE_BETA SE_TSS DOC_MANAGEMENT FLOEFD 3D-SKETCH SIMULATION Teamcenter Share TECH_PUB ASSEMBLY APPLICATION PART/SHEETMETAL TRANSLATORS DRAFT SETUP AUTOMATION FLOMASTER C2O HELP Solid Edge Marketing

Summary


Details

March 18, 2024

Dear Solid Edge Customer:

Solid Edge 2024 Update 4 is now available for download.

We appreciate your continued business and participation in the software support process. Your feedback helps us improve Solid Edge and better serve your business needs.

Sincerely,

The Solid Edge Team

============

Release Notes:

============

Solid Edge 2024 Update 4

Version: 224.00.04.04

Download Solid Edge 2024 (2310) Updates

If clicking the direct download URL does not resolve in your browser, please go ahead, and navigate from the top-level Support Center.

===============

Email Notification:

===============

To receive direct email notifications for Solid Edge Updates, navigate to your Support Center Profile (https://account.sw.siemens.com/profile, scroll to Newsletter Subscriptions, and check the box for Software Field Bulletin

==========================================

This Solid Edge Update resolves the following PRs:

==========================================

===Assembly===

PR 10745929: Adding another control point on a 3D curve causes the curve to be misaligned.

PR 10747951: When guided with the route command, the 3D curve loses its tangent constraint.

PR 10893167: A drawing does not update due to assembly features not automatically recomputing.

PR 10902318: Unable to place an elbow at the corner of a 3D sketch.

PR 10910085: Holes are not highlighted in the Pattern feature step.

PR 10914953: Performance issues related to making a part adjustable.

PR 10971651: Fastener Regeneration issue.

PR 10980902: The assembly drawing does not display a sketch from part.

PR 10988412: Problem with parts displaying in assembly.

PR 10860687: Cannot add models and drawings to Design Configurator.

PR 10869082: Show Only is not working correctly with a suppressed occurrence selected.

PR 10995003: The print command is missing in the customize ribbon bar for the assembly environment.

PR 12006614: A cutout feature in the subassembly does not update in the main assembly.

PR 12012546: Solid Edge creates multiple Thread Styles when a default thread style is not set.

PR 12013583: Solid Edge crashes when importing a point cloud.

PR 343846: Print Validation of an ASM crashes after creating an FOA and before saving.

===Draft===

PR 10916573: Family of Assembly (FOA) and its associated drawings are never up to date.

PR 10937451: Solid Edge is being closed because the system is low on memory.

PR 10940045: Solid Edge crashes when converting to a Draft view.

PR 10938988: BOM shows parts that should be in a single line, in multiple lines.

===Part/Profile/Sheetmetal===

PR 10969242: Color display is incorrect when "Physically based rendering" is disabled.

PR 10842530: Setting a dimension tolerance in Solid Edge 2024 is much different than in 2023.

PR 10890538: When a symmetric by-axis relation is applied to two circles, the dimension between them becomes driven (blue).

PR 10893073: Editing dimensions in a fully constrained profile causes all dimensions to fail.

PR 10893801: Solid Edge crashes when regions of a meshed body are automatically identified.

PR 10808630: Solid Edge crashes when selecting 'Align' and 'Delete Mesh' in the Reverse Engineering tab.

PR 10852686: A feature in FOP members fails in Solid Edge 2023, while it works well in Solid Edge ST9.

PR 10876139: Solid Edge crashes when redefining the diameter of a Hole to a value that is too large or invalid.

PR 10880296: Solid Edge crashes when pressing 'Win+shift+s' on the keyboard for screen-print.

===SEEC===

PR 389570: Added Teamcenter 2312 server support for Solid Edge.

PR 10853494: Duplicate command in Active Workspace is resetting the Item and Item Revision names.

PR 10983489: Native Solid Edge shows Embedded Client Teamcenter login window when inserting Standard Parts.

PR 10987838: Solid Edge is showing a new version of an Assembly.

PR 10946369: Solid Edge crashed during part replacement with the copy and edit-in-place command.

===Solid Edge Data Management===

PR 10905336: Switching automatic numbering off/on will reset to hardcoded values.

===TechPub===

PR 10953447: The hyperlinks are not correctly generated in the PDF table of contents.

PR 10953432: Technical Publication crashes while saving .qsd file after check-out & check-in.

PR 10993265: An error occurs after updating a model in Publishing 2024.

PR 10993610: The inactive area in the "Select Markup" environment is not selectable.

PR 10993872: Functions not working correctly in an HTML file.

PR 11019687: Poor highlighting of small details in the HTML file.

===Translators===

PR 10851335: Pro E data migration is not working.

PR 10838049: Material transfer from Solid Edge to NX is not working as expected.

PR 10879634: Inventor migration is failing.

KB Article ID# PL8781813

Contents

SummaryDetails

Associated Components

L10N: ALL