Needs help with data import into Teamcenter.

2024-04-08T15:09:56Z

Summary


Details

When importing data into Teamcenter performance can be poor as the import tools search for files across the vault located on the network. Is there a way to have the data prep tools and the add to Teamcenter tools use Microsoft's fast search indexing?

Platforms
  • INTEL windows-1064
Release Versions
  • Solid Edge V224.0
Solution

No, the dataprep and add to Teamcenter tools do not use Microsoft's fast search capabilities.When prepping data and adding data to Teamcenter, use a single folder if possible to reduce the time files are searched for. It also helps reduce the number of duplicate files during the prepping process by identifying duplicate file names for the user as the files are added to the single folder.

Notes

KB Article ID# PL8781788

Contents

SummaryDetails

Associated Components