The Browse button is Missing on the Output File Menu when Postprocessing

2024-03-27T15:25:11Z

Summary


Details

When posting a CAM program a UGII_CAM_SETUP_ROOT_DIR undefined menu with the message UGII_TEMP_DIR will be used to output CAM data is displayed. What is causing this?


Platforms
  • INTL64 windows-764
Release Versions
  • NX V2312
Solution

This message indicates that the Configuration is a Cam Library type. To confirm this expand the Postprocessor Output File menu and check to see if the Browse button is missing. A picture of this missing option can be seen in the menu below.


To temporarily change the Configuration go to File -> Preferences -> Manufacturing -> Configuration.


Press the Browse button to navigate to the cam_general Configuration.


Setting the Configuration to CAM General will display the following menu. Notice the Browse button is now available.


Notes

KB Article ID# PL8779437

Contents

SummaryDetails

Associated Components