Saving assembly raises the error "there were errors importing assembly arrangement PLMXML document to Teamcenter"

2024-03-14T19:13:16Z

Summary


Details

Symptom

---------

From NX Syslog:

++++++++++++++++++++++

Error: 940598, (TC 0): There were errors importing assembly arrangement PLMXML document to Teamcenter.

Total save time: CPU time: 3.423 secs, Real time: 7.183 secs

&MACRO FOCUS CHANGE IN 1

&MACRO MESSAGE_BOX -2, No attempt was made to save the following parts.

&MACRO MESSAGE_TEXT Use the assembly navigator 'Refresh Teamcenter Information' command to update the modifiable column

&MACRO MESSAGE_TEXT

&MACRO MESSAGE_TEXT and see why you are not able to save these parts.

&MACRO MESSAGE_TEXT It is also possible that you do not have write a

&MACRO MESSAGE_TEXT ccess to the item in Teamcenter.

++++++++++++++++++++++

Solution

Ensure Customer Default "Synchronize assembly arrangements" is OFF

Teamcenter Integration -> General -> Assembly

Set "TC_arrangement_error_when_used_anchor_not_found" set as Site Preference to 0.

This preference controls the behavior of assembly arrangement creation in the event that a used arrangement anchor is not found in a child assembly.

0 = create the arrangement even though a used arrangement is not found on a child assembly (The default value = 0).

1 = do not create the arrangement but return an error status

KB Article ID# PL8779187

Contents

SummaryDetails

Associated Components