Solid Edge 2310 Export Nest

2024-08-15T10:57:00Z

Summary


Details

Would prefer to see all nested sheets (tables) in the exported dxf file. When using NestFab, unclicking the Show Unique Nests Only box was giving them a full set of tables upon export.

Platforms
  • na windows-1064
Release Versions
  • Solid Edge V224UPD6
Solution

You need to add a setting to the settings.ini file: Add [NestSettings] if missing and add SheetGap = 0 under it.

Notes

KB Article ID# PL8778753

Contents

SummaryDetails

Associated Components