How to Reset all Drawing Dimensions to a Drafting Standard

2024-03-18T17:44:01Z

Summary


Details

How to Reset all Drawing Dimensions to a Drafting Standard.

Solution

 See above video for procedure to reset all drawing dimension to a drafting standard.

How to Reset Dimensions to Drafting Standard

1.       In the Top Border Bar, set the Type Filter to Dimension.

2.       Select all the dimensions that need to be reset.

-          Note: To select all dimensions, in the Top Border Bar choose Select All or Ctrl+A.

3.       Right click a highlighted dimension and select Settings.

4.       In the Settings dialog, under the Inherit group, change Settings Source to Customer Defaults.

5.       Click Load from Settings Source.

6.       Click Close.

-          Note: This can be done to other drafting entities, such as Notes or Symbols and will reflect the drafting standard as set in Customer Defaults.

KB Article ID# PL8778376

Contents

SummaryDetails

Associated Components