Reversing the Material Side in a Contour Profile Operation

2024-03-15T20:40:13Z

Summary


Details

A Contour Profile operation is used to create a tool path on Sheet Bodies. Because the faces being cut are Sheet Bodies and not a Solid Body the surface vectors can be in either direction. This could cause the tool to cut on the wrong side. How can the surface vectors be reversed if incorrect? 


Platforms
  • Windows 11
Release Versions
  • NX V2312.4000
Solution

After selecting the Part Geometry press Topology.


On the Topology menu press Rebuild Topology and Unify All.


  Press Reverse All to correct the surface vector. 


After correcting the surface vectors the tool is on the correct side of the sheet.


Notes

KB Article ID# PL8777723

Contents

SummaryDetails

Associated Components