"Clean Motion Object" in Part Cleanup is not memorized in the dialog

2024-03-12T00:09:24Z

Summary


Details

After checking and executing "Clean Motion Objects" in Part Cleanup, I tried to run Part Cleanup again, but it was unchecked. It doesn't seem to be memorized in the dialog.

Reproduced Steps:

1. Open a part

2. File > Utilities... > Part Cleanup... > Clean Motion Objects=ON > OK

3. Again perform Step 2 above


Solution

This behavior is due to NX problem and is fixed in NX 2406.

Workaround: check it on each time.

Notes

**Please refer to PL8777281 for Japanese article.

Release Versions
  • Simcenter 3D Solutions V2306
  • NX V2306
Platforms
  • Windows x64 10
  • Windows x64 11

KB Article ID# PL8777282

Contents

SummaryDetails

Associated Components