Measure command was performed in the middle of View Section command. After that, when finish Measure command, the control does not return to View Section command and the command terminates.
Reproduced Steps:
1. Assembly tab > Sections > Mouse right click > New Section...
2. Analysis tab > Measure > Cancel
View Section command terminates:
The behavior is due to NX problem, and it is fixed in NX 2406 and NX 2312.6000.
Workaround: There is no effective workaround, so please measure using Measure command in advance.
Notes**Please refer to PL8777218 for Japanese article.