Unable to set font for PMI Notes using MBD rules

2024-03-05T02:48:32Z

Summary


Details

There is "Create Note" rule in the MBD Logical Rule Library, but I can't find an option to set the text font for the PMI Notes that are created. Is it possible to set it within the rules?

Reproduced Steps:

1. PMI tab > Define > Open > MBD Logical Rules>Note > Create Note


can't find an option to set the text font for the PMI Notes:


Solution

There is currently no option to set this within the rule. It will be entered in the font specified in advance by the PMI preferences.

Notes

**Please refer to PL8777216 for Japanese article.

Release Versions
  • NX V2007
  • NX - MBD V2007
Platforms

    KB Article ID# PL8777217

    Contents

    SummaryDetails

    Associated Components