NX I want to display command help in an external browser

2024-03-05T02:36:24Z
NX System Administration

Summary


Details

When pressing F1 key on the dialog while performing a command, NX help is displayed in NX's embedded browser or in an external browser such as Google Chrome. This behavior is different depends on the commands. For example, "Extrude" is displayed in the embedded browser and "Block" is displayed in an external browser. Is it possible to control where it is displayed through settings?

Extrude:


Block:


Solution

Currently, the display browser of the help is controlled within the NX system, so it is not possible to change it through settings.

Notes

**Please refer to PL8777214 for Japanese article.

Release Versions
  • NX V2306
  • NX - UGDOC V2306
Platforms
  • Windows x64 10
  • Windows x64 11

KB Article ID# PL8777215

Contents

SummaryDetails

Associated Components

Documentation