Textures are not retained in 3MF Import/Export

2024-03-05T01:26:48Z

Summary


Details

When using NX 3MF translator and importing a 3D manufacturing format (.3mf) file, the geometries are imported and displayed correctly, but the textures are not retained.

Reproduced Steps:

1. Open a part

2. File > Import(Export) > 3MF


Solution

The behavior is working as designed.

NX supports import/export of 3MF data, but does not support texture data, so although shapes are imported, texture data cannot be retained (imported/exported).

In NX, please use the Studio Materials functionality to assign new Visualization Material.

Notes

**Please refer to PL8777210 for Japanese article.

Release Versions
  • NX V2306.7000
  • NX - TRANSLATOR V2306.7000
Platforms
  • Windows x64 10
  • Windows x64 11

KB Article ID# PL8777211

Contents

SummaryDetails

Associated Components