The Solid Edge Electrical project becomes read only

2024-04-01T06:37:29Z

Summary


Details

Solid Edge Electrical project becomes read only, cannot open diagram for edit. Shows an error as,

"Cannot Open diagram for edit, open-read-only?

User 'System' has been editing the diagram since 'MMM DD, YYYY, HH:MM AM'

Either open in read-only or select cancel and wait until other user has finished editing this design"

Solution

Solid Edge Electrical has an option that apply a lock to user account to avoid data corruption in case or random termination/ closure of Solid Edge Electrical application.

Check the option "Enable clear locks on user account" is checked/ unchecked?

If this option is selected, it allow the current user to release locks on their own user account.

CAUTION:

Locks should only be removed from user's accounts and projects when the user is effectively not working on the data, for example, following an unexpected client close down. Removing a lock in other circumstances will cause database corruption and render projects and designs unusable and unrecoverable.


You can find this option under Solid Edge Wiring Design application > Solid Edge > System > System Preferences


Notes

10878143

KB Article ID# PL8777165

Contents

SummaryDetails

Associated Components