Solid Edge In Solid Edge the hide option is not displayed

2024-04-01T06:36:54Z
ASSEMBLY

Summary


Details

Sometimes hide option was not showing and sometime context tool bar was also not showing

There are some missing file but hide option should be there irrespective of missing component.

Solution

The part doesn't show hide option needs to be updated from update all open parts. The 'update all' forces the subassembly, parts and assembly patterns to update.

The Update All Open Documents command updates an assembly when you edit a part in the context of the assembly. For example, with Automatic Update on, if you in-place activate a part from an assembly and edit the value of a driving dimension, the changes are automatically applied to the part but not to the assembly. You can use this command to update the assembly.

You can also use this command to update a part copy from within the assembly.

After updating the part, the hide option is displayed for the part.

Notes

10871479

KB Article ID# PL8777164

Contents

SummaryDetails

Associated Components

ASSEMBLY: OTHER