Solid Edge Types of Solid Edge Licenses

2024-03-08T10:55:50Z
SETUP

Summary


Details

This article applies to Solid Edge Licensing and describes the various types of licenses available.

Solution

Siemens PLM supports two basic types of authorization codes (licenses) that support a variety of contract models and configurations.

Node Locked licenses can be locked to a hardware Composite ID and do not require a license server as they are "uncounted".  You simply point the applications to the plain text license file using an environment variable.  The applications read the license file upon invocation and determine if you are authorized to run them.

Example of a Node Locked license/authorization code:

FEATURE solidedgeclassic ugslmd 224.0 14-mar-2024 uncounted \ HOSTID=COMPOSITE2=7B654B163F98 asset_info=Projektgruppe \ START=15-feb-2024 TS_OK SIGN="1E6D 6674 5557 A8BE 6EDE 0608 \ A902 18A1 16DD 1AE3 F4DA 6BD1 657E 44D1 AC86 036B 741B 9A66 \ 9E55 855F D3EA 55A3 E933 81EB 69FB 2768 C43F 974C 5521 8C01"

A Floating license can be used by any computer on your network.  Because floating licenses are "counted", you must run a license server. A Composite ID (CID), Ethernet address or a hardware key can be used as the server id for your floating licenses.  Applications are directed to the license server using an environment variable and make requests for license features upon invocation.  Because the applications periodically check with the license server within the application's session to determine if they are still licensed, the use of floating licenses requires a persistent network connection with the license server.

Example of a Floating license/authorization code:

SERVER licman COMPOSITE=1C9D0072E6AA 28000 VENDOR saltd PORT=28001 INCREMENT solidedgeacademicu ugslmd 224.0 26-feb-2025 50 \ VENDOR_STRING="SOLID EDGE ACADEMIC COPY" SUPERSEDE \ DUP_GROUP=UHD user_info="Common to SE Acad Perpetual License; \ Solid Edge Master Academic Bundle" ISSUED=26-feb-2024 \ BORROW=2880 SIGN="0207 3696 97B1 F89F 9128 2343 9FE7 1D7E B706 \ 2046 BB27 4205 D1AC 8C68 104C 140A CAD4 BBF6 DB05 04A4 D622 \ C5C8 B47F E8C9 9B57 8784 CED2 5B59 388D 7F47"

Please refer to The Flexnet Publisher License Administration Guide for more information on the various fields in a license file.

There is a third, less common type of license called Floating Node Locked that functions in much the same way as a Floating license, in that you must run a license server.  However, unlike a Floating license that can be used by any host on your network, Floating Node Locked licenses can only be checked out by one specific machine.  This is controlled with a COMPOSITE2 field in the INCREMENT line.

Example of a Floating Node Locked license/authorization code:

SERVER licman COMPOSITE=1C9D0072E6AA 28000 VENDOR saltd PORT=28001 INCREMENT solidedgeclassic ugslmd 224.0 16-mar-2025 1 9ED3261677742A84B49D \ VENDOR_STRING=259CD3E2 HOSTID=COMPOSITE2=7B654B163F98 SN=42049388 SIGN2="0276 \ 9247 47DE 268C 290A ACB7 7351 D49A 8CB1 019C 64B4 0074 17B2 4442 7346 \ 1659 A6F3 6B71 D646 36DD 4504 A7A6 6D82 D6F0 BC0D 2170 B266 878B 17B4 \ DC07"

KB Article ID# PL8777158

Contents

SummaryDetails

Associated Components

SETUP: LICENSING