Solid Edge 2023 Update 0011 Announcement

2024-02-26T22:24:14Z

Summary


Details

February 26, 2024

Dear Solid Edge Customer:

Solid Edge 2023 Update 0011 is now available for download.

We appreciate your continued business and participation in the software support process. Your feedback helps us improve Solid Edge to serve your business needs better.

Sincerely,

The Solid Edge Team

============

Release Notes:

============

Solid Edge 2023 Update 0011

Version: 2210.0011.004 x64

Download Solid Edge 2023 (2210) Updates

Note: if the direct download URL doesn't resolve in your browser, please navigate from the top-level Support Center.

===============

Email Notification:

===============

To receive direct email notifications for Solid Edge Updates, navigate to your Support Center Profile (https://account.sw.siemens.com/profile, scroll to Newsletter Subscriptions, and check the box for Software Field Bulletin

==========================================

This Solid Edge Update resolves the following PRs:

==========================================

===Assembly===

PR 10883149: Solid Edge Motion is giving false data output.

PR 10340553: A PWD component is not displayed in a draft view.

PR 10783895: Incorrect position of mirrored components after opening.

PR 10843587: Frame components are not visible.

PR 10865266: An internal component does not show any feature, so it cannot be edited.

PR 10870275: Crash while working with Weldment assembly.

PR 10898682: Assembly pattern does not update.

PR 10902087: crash when opening some assemblies more than once.

PR 10909602: Solid Edge 2023 Crash on Tube Edit Definition Options.

PR 10939613: non-reproducible crash

PR 12006609: Sketch in assembly hole feature moves away unexpectedly.

PR 12006611: Upon updating or recompiling, holes in the assembly feature move away.

PR 10889293: Assembly relationship fails automatically.

PR 10893034: Mirror fault with Frame component

PR 10947199: Pattern of another pattern with frame

PR 12008300: Termination for delete tube.

PR 10902318: Problems with user parts (straight union type) in XpresRoute pipe routes

PR 10971651: fastener Regeneration issue.

PR 10980902: The assembly drawing does not display a sketch in part.

PR 10988412: Problem with parts displaying in assembly.

PR 10787598: Issue with renaming a Design Configurator project, including drafts.

PR 8690361: Solid Edge 2023 is crashing frequently.

PR 343846: Solid Edge crash on Print Validation of ASM after creating FOA before saving.

===Draft===

PR 10889922: actions in and with the view properties dialog of a specific draft file last version

PR 10896922: Breakout on hole causes a reproducible crash.

PR 10840405: Synchronous Simplify Curve dialog disappears when launched.

===Part/Profile/Sheetmetal===

PR 10517441: File Repair - Make sure the file is the correct type and version for the application.

PR 10919561: Solid Edge crashes when marking a single region of the mesh body with a red color.

PR 10919811: Solid Edge crashes when changing the display order of a sketch containing symmetry.

PR 10887802: The list of Hole Settings is not displayed normally.

PR 10969242: Color display is incorrect when "Physically based rendering" is disabled.

===SEEC===

PR 10784149: Assembly downloads take a long time.

PR 10864151: The SEEC Diagnostic app is not running with the Mech Design bundle license.

PR 10983489: Native Solid Edge shows SEEC-TC logon window to insert STD Parts.

PR 10987838: Solid Edge is showing a new version of Assembly.

PR 10946369: Solid edge crash issue

PR 389570: Teamcenter 2312 server support for Solid Edge.

===Data Management===

PR 10745180: Search (Listing) by Properties in SEDM Server/Client env to slow.

PR 10905336: Switching automatic numbering off/on will reset it to hardcoded values.

PR 10918825: SE crashes when entering the page number and then clicking the next page in the file search result.

===TechPub===

PR 10953447: The hyperlinks are incorrectly generated in the PDF table of contents.

===Translators===

PR 12000081: Empty files are migrated for Creo Element Direct Migration

PR 10851335: Pro E data migration is not working.

KB Article ID# PL8777147

Contents

SummaryDetails

Associated Components