Cannot rotate Simulation Force direction

2024-03-07T16:39:33Z

Summary


Details

I want to rotate the direction of a Force with the Steering Wheel and set the Angle in Solid Edge Simulation.

Unfortunately I cannot rotate the steering wheel.  How to set the direction?

Platforms
  • Windows x64 11
  • Windows x64 10
Release Versions
  • Solid Edge V224.0
  • SOLID_EDGE - SIMULATION V224.0
Solution

When you place the Force, select the Steering Wheel center and place it.

To set the angle, use 'shift+click' on the Steering Wheel Torus.  Then you can set the angle.


See also https://docs.sw.siemens.com/en-US/doc/246738425/PL20220830878154140.validate/fem_simplify01

Notes

KB Article ID# PL8776589

Contents

SummaryDetails

Associated Components