How to set up icon on toolbar that enable selection of different model view orientation

2024-03-07T15:38:16Z

Summary


Details

Currently the activation and display of certain model view orienation can be initated via:

(1) Right Mouse Button (RMB) on the screen area, click "Orient View"


OR

(2) Using Part Navigator panel and expand Model View node


Question: Is there a way to have the above methods configured on the toolbar area?

Solution

(1) Go to "Menu > Tools > Customize..." to bring up the Customize dialog.

(2) In the Commands tab, under the Categories area, find and highlight "All Dropdowns" (no need to expand this option).

(3) On the right-hand side in the Items area, locate "Orient View Drop-down" and drag it out to drop it in the desired area on the ribbon.


KB Article ID# PL8776451

Contents

SummaryDetails

Associated Components