Tecnomatix Tecnomatix Controllers for CLS_UPLOAD

2024-05-10T04:28:31Z
Process Simulate

Summary


Details

Dear Siemens Digital Industries Software Customer,

We are pleased to inform you that Tecnomatix controllers for "CLS_UPLOAD"

are available for download from https://support.sw.siemens.com.

See Tecnomatix_<ControllerName>_changes_log.html for details concerning this update.

Note: This file is located in the 'Robot Controllers Change Logs' folder directly under the 'Tecnomatix <Version> Robot Controllers' folder.

Use the following steps to download:

- Login to https://support.sw.siemens.com

- If you do not have an account, click 'Register Now' and fill out the information.

- Once on Support Center, if you do not see Tecnomatix under 'My Products', click 'Manage Products'.

- Scroll down and toggle On the Tecnomatix product.

- Scroll back to the top and click Support Center in the breadcrumb.

- Select 'Tecnomatix' from 'My Products'

- Select 'Download'

- Select Tecnomatix 16.1, 16.1.1, 16.1.2, 17.0, 2206, 2301, 2307 or 2402

-Select Tecnomatix 16.1 Robot Controllers, Tecnomatix 16.1.1 Robot Controllers, Tecnomatix 16.1.2 Robot Controllers, Tecnomatix 17.0 Robot Controllers, Tecnomatix 2206 Robot Controllers, Tecnomatix 2301 Robot Controllers, Tecnomatix 2307 Robot Controllers or Tecnomatix 2402 Robot Controllers

Download the file(s):

Tecnomatix_16.1_CLS_UPLOAD_64BIT_v1.15.3_09_05_2024.exe

Tecnomatix_16.1.1_CLS_UPLOAD_64BIT_v1.15.3_09_05_2024.exe

Tecnomatix_16.1.2_CLS_UPLOAD_64BIT_v1.15.3_09_05_2024.exe

Tecnomatix_17.0_CLS_UPLOAD_64BIT_v1.15.3_09_05_2024.exe

Tecnomatix_2206_CLS_UPLOAD_64BIT_v1.15.3_09_05_2024.exe

Tecnomatix_2301_CLS_UPLOAD_64BIT_v1.15.3_09_05_2024.exe

Tecnomatix_2307_CLS_UPLOAD_64BIT_v1.15.3_09_05_2024.exe

Tecnomatix_2402_CLS_UPLOAD_64BIT_v1.15.3_09_05_2024.exe

To Install:

Place Tecnomatix_<TecnomatixVersion>_<ControllerName>_NNBIT_vVV_MM_DD_YYYY.exe into a folder ($Tecnomatix/downloads is suggested, where $Tecnomatix is the full path to the Tecnomatix installation).

Run Tecnomatix_<TecnomatixVersion>_<ControllerName>_NNBIT_vVV_MM_DD_YYYY.exe.

The default installation point is C:\Program Files\Tecnomatix.

If you have any issues with the installation or support of these fixes,

please contact your local GTAC support group.

Sincerely,

Siemens Digital Industries Software

KB Article ID# PL8791069

Contents

SummaryDetails

Associated Components

Process Simulate Off-Line Programming (OLP)