Cannot generate valid floating license file for Solid Edge 2019 or earlier

2024-07-30T16:53:23Z

Summary


Details

This article addresses being unable to successfully generate a valid floating license file for Solid Edge 2019 and prior versions.  The use cases in which you would want to generate a new Solid Edge 2019 license file include, but are not limited to the following: 

  • Customer wants to generate a new license file and use it with a hardware dongle.
    • Customer has ordered additional Solid Edge products but wants to work with Solid Edge version 2019 or earlier.
      • The customer has chosen the XaaS maintenance model but is still working with Solid Edge version 2019 or earlier.
        • Customer wants to upgrade their product from Foundation to Classic for example and are still using  Solid Edge version 2019 or earlier.
          • Customer needs to change or update the registered server details.
            Solution

            If a customer wants to run a Solid Edge version that is prior to Solid Edge using the Common Licensing Toolkit (CLT) then the customer must own legacy a Solid Edge product that allows for creating a license against a Host ID/MAC address.

            The version of Solid Edge that started supporting CLT was Solid Edge 2020.  Solid Edge 2019 and earlier versions do not support CLT.

            New valid floating license files for Solid Edge 2019 and earlier versions can only be generated if the core base Solid Edge products are identified as "unique host id" products.  If the core base Solid Edge products are not unique host id products then it is not possible to generate a new valid floating license file for Solid Edge 2019 or earlier versions.

            In order to generate a valid floating license for Solid Edge 2019 or earlier versions the customer must either own, purchase, or trade in their CLT Solid Edge products for the comparable Solid Edge products with the unique host id method as listed in the Pricebook:

            • SE388H: Solid Edge Premium - Floating (Unique Host ID Method)
              • SE320TC: Solid Edge Classic - Floating (Unique Host ID Method)
                • SE351H: Solid Edge Foundation - Floating (Unique Host ID Method)
                  • SE397H: Solid Edge P&ID Design - Unique HostID
                    • SE398H: Solid Edge Piping Design - Unique HostID
                      • SE399H: Solid Edge Piping Design Add-on - Unique HostID

                        This is fully documented in the Pricebook where for these products, it clearly states the following:

                        This is a legacy product that should only be used in sales situations involving customers wanting to run Solid Edge 2019 and prior versions.

                        It is important to note

                        Ordering a core base product that is not from the list above and trying to run Solid Edge 2019 or earlier will result in a non valid license file being generated 

                        For Solid Edge 2020 and newer versions please order the appropriate concurrent usage product.

                        Notes

                        If you have further inquiries about Solid Edge Floating Licensing please refer to the FAQs collection link below:

                        Solid Edge Floating License FAQs Collection

                        KB Article ID# PL8775294

                        Contents

                        SummaryDetails

                        Associated Components