Solid Edge Solid Edge Floating Licensing FAQs Collection

2024-08-05T05:18:22Z
SETUP

Summary


Details

This FAQs collection is intended to provide an overview of relevant Solid Edge Floating Licensing FAQs, sorted by categories "About", "How To/Guides", and "Troubleshooting".    

This is a living document, which means that new FAQs and categories may be added to this collection.

Solution

About Solid Edge Floating Licensing

FlexLM License server for Solid Edge on Linux 

Where do I find the FlexNet License Administration Guide?

What is a Solid Edge Unique Host ID License?

Can you use a Dongle on a Solid Edge Floating License with a Virtual server?

Supported Platforms Overview and Roadmap for Siemens License Server 

How to not consume a Floating License while borrowing another for Solid Edge

Home Use Licensing Eligibility for Siemens Mechanical Design Bundles

What are the certified platforms for Solid Edge FlexLM License server located in the Cloud?

Ports in License Management / FlexLM (needed for Firewall settings)

Which FlexLM License Server will work with Solid Edge 2024 ?

What license server do I install for Solid Edge 2023?

What are the supported License Server operating systems for 2022

What version of the FlexNet software does Solid Edge 2019 use?

What is the name of the Options File for a Floating License in Solid Edge 2020 ?

Does SEFlexlm support Windows 2016 server?

Deploy one license file on 2 servers

Question on upgrading license server from ST9 to SE2021

Return a borrowed license if borrowing user or workstation is no longer available

Is the Solid Edge 2019 FlexNet License Manager supported on a 32 Bit Platform?

Can there be Solid Edge Floating Licenses and Node Locked licenses in the same license file

On a floating installation does Data Prep tool checkout a license?

How to Configure Floating Licensing 

How to update a license file on an existing FlexLM License Server

How to update a FlexLM License Server?

How to RESERVE a license in flexlm options file

What is the correct Directory for the ugslmd Options File "ugslmd.opt" ?

Who has licenses checked out and how many?

Licensing Usage, Current List Used and User

FlexLM timeout option TIMEOUT with Floating Licensing

License Borrowing with SE2020

How to not consume a Floating License while borrowing another for Solid Edge

How to define the variable SELMD_LICENSE_FILE

How to manually start/stop/restart FlexLM License Manager?

Controlling the Order of Listed Network Adapters in GetCID Output

Define the Solid Edge license server on a client workstation

Determining if a License is Borrowed

Easily stopping and starting the FlexLM License Manager

How to prevent 2D user from checking out a Solid Edge Classic license

Can a TRIAD license server be setup for Solid Edge 2021?

Request to switch from NodeLocked to Floating Licenses

Configure client with different license servers for Solid Edge and Teamcenter

Obtaining a floating Solid Edge license over a VPN or WAN

How can a Solid Edge bundle be "broken" for license borrowing?

Forcing the return of a borrowed license

Troubleshooting Floating Licensing

Cannot generate valid floating license file for Solid Edge 2019 or earlier

Possible FlexLM problems after updating the operating system

License Manager Server is down. How to keep users working?

Composite Hostid (CID) changing when switching WiFi 

FlexNet Licensing error:-15,10. System Error: 10013 "WinSock: Access denied"

getcid returns "no Siemens Software Licensing Composite HostID"

Easily stopping and starting the FlexLM License Manager

Increased License Usage after Updating to Newer Versions of Solid Edge

Using .bat files for SE license checkout in floating installation

Solid Edge Classic Plus licenses cannot be checked out from the license server

License Error, License server version is older than the client

License server not running with new license (added seat)

License Manager quit working on server.

FlexLM License Server will not start during Configuration

Borrowed license will not return

Floating license is not working.

Solid Edge license error: Cannot check out an uncounted license within windows terminal.

Solid Edge License Server will not run

Problem borrowing a License in Solid Edge 2019 and earlier

Cannot run NX or SE2020 from license server.

SEWinDongleID executable reports "No Hardware Key detected" on License Server

Unable to read the Solid Edge 2019 FlexNet License Manager Server from the Solid Edge Client machine.

Intermitent problem with remote users connecting to Solid Edge FlexNet License Manager.

Error 1.5.-124 attempting to return a borrowed license early

Bad message command and FlexNet licensing error: -140, 148

Notes

If you have further inquiries about Solid Edge Licensing please refer to the FAQs Collection link below:

Solid Edge Licensing FAQs Collection

KB Article ID# PL8775006

Contents

SummaryDetails

Associated Components

SETUP: LICENSING