Tecnomatix setup detects unsuitable Oracle version.
Error: "Setup has detected that your current Oracle version is not suitable for installing eMServer"
First make sure the Oracle version is supported. In the documentation section, see either the "Tecnomatix Installation on eMServer" or the "Tecnomatix Administration" guide for details.
Then in the system path, there should be a path that points to the Oracle client bin directory; this is where the oci.dll resides, which is used by Tecnomatix the setup.
Notes