NX UGCAMTemplateData dataset is not in the TC Environment

2024-02-19T12:52:11Z
NX for Manufacturing

Summary


Details

UGCAMTemplateData data set is missing from Teamcenter. It's possible to  receive the following error...

"The "manufacturing_access" component license is needed"

Solution

If the folder owner is infodba and the dataset UGCAMTemplateData is missing, the customer can run the following command in a Teamcenter cmd window:

nxmgr_add_note_types -u=infodba -p=${TC_USER_PASSWD} -g=dba

KB Article ID# PL8774669

Contents

SummaryDetails

Associated Components

TC for Manufacturing