Solid Edge 2024 Update 3 Announcement

2024-02-12T19:22:58Z

Summary


Details

February 12, 2024

Dear Solid Edge Customer:

Solid Edge 2024 Update 3 is now available for download.

We appreciate your continued business and participation in the software support process. Your feedback helps us improve Solid Edge to serve your business needs better.

Sincerely,

The Solid Edge Team

============

Release Notes:

============

Solid Edge 2024 Update 3

Version: 224.00.03.04

Download Solid Edge 2024 (2310) Updates

Note, if the direct download URL doesn't resolve in your browser, please navigate from the top-level Support Center.

===============

Email Notification:

===============

To receive direct email notifications for Solid Edge Updates, navigate to your Support Center Profile (https://account.sw.siemens.com/profile, scroll to Newsletter Subscriptions, and check the box for Software Field Bulletin

==========================================

This Solid Edge Update resolves the following PRs:

==========================================

===Assembly===

PR 10340553: A PWD component is not displayed in the draft view.

PR 10865266: An internal component is not showing features.

PR 10888548: Ground relation lost after part when center plane relation is suppressed.

PR 10902087: Crash occurs when activating an assembly with decals.

PR 10783895: Mirrored components are positioned incorrectly after opening the assembly.

PR 10870275: Solid Edge crashes during fillet weld creation

PR 10939613: non-reproducible crash

PR 12006609: Sketch in assembly hole feature moves away unexpectedly.

PR 12006611: Some features in this file move after updating/recomputing.

PR 12008300: Assembly with tubes crashes when editing.

PR 10893034: The user cannot mirror a frame part whose parent file only has a cross-section.

PR 10947199: The user cannot Pattern a frame pattern.

PR 10889293: Assembly relationships fail in this assembly, and some parts disappear.

PR 10955568: Solid Edge closes when a relationship is deleted.

PR 10958192: Solid Edge crashes when creating an assembly feature cutout with "Create Synchronous Cuts..." enabled.

PR 10883149: Solid Edge Motion is generating invalid output.

===Draft===

PR 10889922: Opening DV properties, Display Tab, Options for list all elements, and then Cancel takes over 1 hour to close.

PR 10892713: Text Scale of Dimension Command resets to 1 each time started.

===General===

PR 10918825: Solid Edge crashes when entering the page number and clicking the next page in the file search result.

PR 12007142: Solid Edge Cloud Enabled Customers, DEX Subscription and Commercial, report a "License expired" message.

===Part/Profile/Sheetmetal===

PR 10889773: It is impossible to edit Physical Thread clearance.

PR 10893433: During a Replace Part operation, Solid Edge freezes or crashes.

PR 10930799: FOP does not update correctly when used as a part copy in another part.

PR 10267714: Profile stuck on screen (edit from ASM) after adding a symmetric relationship.

PR 10777191: Application Crash due to Solid Edge Status Setting via Apprentice API in AddIn

PR 10919811: Solid Edge crashes when moving the object up in the display order.

PR 10950107: Chinese Solid Edge subdivision modeling cannot display the segment value in the Box dialog.

PR 12001125: Some Japanese characters are displayed in incorrect locations on the Smart Dimension dialog.

===SEEC===

PR 10784149: Assembly downloads are taking a long time.

===Solid Edge Data Management===

PR 10745180: Search (Listing) by Properties in SEDM Server/Client env to slow.

===Translators===

PR 12000081: Empty files are migrated for Creo Element Direct Migration

PR 385106: Unable to Open NX 2312 Files in Solid Edge 2023 and 2024

KB Article ID# PL8774661

Contents

SummaryDetails

Associated Components