Dear Siemens Digital Industries Software Customer,
We are pleased to inform you that Tecnomatix controllers for "EFORT_XPL"
are available for download from https://support.sw.siemens.com.
See Tecnomatix__changes_log.html for details concerning this update.
Note: This file is located in the 'Robot Controllers Change Logs' folder directly under the 'Tecnomatix Robot Controllers' folder.
Use the following steps to download:
- Login to https://support.sw.siemens.com
- If you do not have an account, click 'Register Now' and fill out the information.
- Once on Support Center, if you do not see Tecnomatix under 'My Products', click 'Manage Products'.
- Scroll down and toggle On the Tecnomatix product.
- Scroll back to the top and click Support Center in the breadcrumb.
- Select 'Tecnomatix' from 'My Products'
- Select 'Download'
- Select Tecnomatix 2301, 2307, 2402 or 2408
-Select Tecnomatix 2301 Robot Controllers, Tecnomatix 2307 Robot Controllers, Tecnomatix 2402 Robot Controllers or Tecnomatix 2408 Robot Controllers
Download the file(s):
Tecnomatix_2301_EFORT_XPL_64BIT_v1.22_14_02_2025.exe
Tecnomatix_2307_EFORT_XPL_64BIT_v1.22_14_02_2025.exe
Tecnomatix_2402_EFORT_XPL_64BIT_v1.22_14_02_2025.exe
Tecnomatix_2408_EFORT_XPL_64BIT_v1.22_14_02_2025.exe
To Install:
Place Tecnomatix___NNBIT_vVV_MM_DD_YYYY.exe into a folder ($Tecnomatix/downloads is suggested, where $Tecnomatix is the full path to the Tecnomatix installation).
Run Tecnomatix___NNBIT_vVV_MM_DD_YYYY.exe.
The default installation point is C:\Program Files\Tecnomatix.
If you have any issues with the installation or support of these fixes,
please contact your local GTAC support group.
Sincerely,
Siemens Digital Industries Software