Using variables to define nominals, receiving errors

2024-02-22T21:04:09Z

Summary


Details

Using variables declared in a macro to define nominals later in the code. The variables are showing as RED in the Inspector window. When the variable is switched to a real number, it works. How can the variables be used successfully?

Platforms
  • INTEL windows-2003_SP2
Release Versions
  • Tecnomatix Quality Management V8.1.0
Solution

The variable was being defined from a FEATURE definition. The use of variables is not supported in FEATURE definitions. Must use real values.

Notes

KB Article ID# PL8773780

Contents

SummaryDetails

Associated Components