Setting decimal places for sketch dimensions

2024-02-07T03:09:31Z

Summary


Details

The option to set the number of decimal places for sketch dimensions is missing from Customer Defaults and Preferences. Please tell me how to set it up.

Solution

The setting uses common option for PMI (Drafting).

Customer Defaults:

File > Utilities > Customer Defaults > PMI > PMI General/Setup > Objects > Coordinate Note > Decimal Places


Preferences:

File > Preferences > PMI > Dimension > Text > Units > Decimal Places


In case of Decimal Places = 2:


Notes

Modeling environment can be accessed from PMI above, but Drafting environment can be accessed from below.

カスタマデフォルト:

Customer Defaults:

File > Utilities > Customer Defaults > Drafting > General/Setup > Standard > Customize Standard > Dimension > Text > Units > Decimal Places


Preferences:

File > Preferences > Drafting > Dimension > Text > Units > Decimal Places


**Please refer to PL8773630 for Japanese article.

KB Article ID# PL8773632

Contents

SummaryDetails

Associated Components