NX Feature name is not displayed in Quick Pick list

2024-02-07T02:37:16Z
NX for Design

Summary


Details

There is a point feature (point “aa”) with an arbitrary name. After performing "Renew Drawing" command, when I tried to select this point object from Quick Pick list when creating dimension, "Existing Point - Point/aa" was not displayed, but "Existing Point - Drafting Point (Extracted Point)" was displayed.

Reproduced Steps:

1. Create a drawing sheet in NX 11 or lower that has a point object with an arbitrary feature name


2. Open the drawing sheet in NX 2306 and perform Renew Drawing

3. Try to create a liner dimension on the point


Solution

This behavior is working as expected.

Due to some enhancements in NX 12, the feature name that is displayed when a point object is selected when creating a dimension has been changed.

Notes

Reference:


**Please refer to PL8773622 for Japanese article.

Release Versions
  • NX V2306
  • NX - DESIGN V2306
Platforms

    KB Article ID# PL8773626

    Contents

    SummaryDetails

    Associated Components

    Drafting