NX If performing Measure command when creating New Section, the section command will end.

2024-03-12T00:06:09Z
NX for Design

Summary


Details

While creating a new section, when Measure command is performed and then finished, control does not return to the section command and the operation ends. For NX 2306 and lower, control returns normally to the section command.

Reproduced Steps:

1. Prepare a model

2. New Section (do not exit command)> performing Measure & finish


** If Measure command finishes, does not go back to Section command.

Solution

This behavior is due to NX problem and is fixed in NX 2406 and NX 2312.6000.

Notes

This problem occurs only in NX 2306 Series.

This behavior occurs both of New Section & edit, but does not occur in PMI Section View.

**Please refer to PL8773620 for Japanese article.

Release Versions
  • NX V2312
Platforms
  • Windows x64 10
  • Windows x64 11

KB Article ID# PL8773621

Contents

SummaryDetails

Associated Components

Modeling