Command line to silently uninstall Solid Edge 2024 Update 2

2024-07-17T08:01:10Z

Summary


Details

What is the command line to silently uninstall Solid Edge 2024 Update 2?

Solution

The command line for Solid Edge 2024 Update 2 (build 224.00.02.004) is:

msiexec /package {FAF68E69-27BE-4111-A3EF-245C40A1C7F2} /uninstall {BF750BCC-8C7A-44A2-A771-C21DBF95E6F0} /qn+ /norestart /log C:\temp\2240002004_uninstall.log

Notes

To the parent article

KB Article ID# PL8773415

Contents

SummaryDetails

Associated Components