Solid Edge Command line to silently uninstall Solid Edge 2024 Update 1

2024-07-17T08:01:04Z
SETUP

Summary


Details

What is the command line to silently uninstall Solid Edge 2024 Update 1?

Solution

The command line for Solid Edge 2024 Update 1 (build 224.00.01.005) is:

msiexec /package {FAF68E69-27BE-4111-A3EF-245C40A1C7F2} /uninstall {2FD4409B-9CB0-4FD8-91CA-7449CEB4ECC6} /qn+ /norestart /log C:\temp\2240001005_uninstall.log

Notes

To the parent article

KB Article ID# PL8773403

Contents

SummaryDetails

Associated Components

SETUP: INSTALL