NX NX Immersive Explorer gives D3DCOMPILER_43.dll was not found

2024-02-28T07:39:56Z
NX for Design

Summary


Details

When starting the NX Immersive Explorer, an error shows:

==================================================================================================
The Code executions cannot proceed because D3DCOMPILER_43.dll was not found. Reinstalling the program may fix this problem.
==================================================================================================

Besides this error, similar errors might show up as well, a list of errors that are cause by the same problem:

==================================================================================================The code execution cannot proceed because X3DAudio1_7.dII was not found. Reinstalling the program may fix this problem.
==================================================================================================

==================================================================================================The code execution cannot proceed because XAPOFX1 _5.dII was not found. Reinstalling the program may fix this problem.
==================================================================================================

==================================================================================================The code execution cannot proceed because XINPUT1_3.dII was not found. Reinstalling the program may fix this problem. ==================================================================================================

Platforms
  • na windows-1064
Release Versions
  • NX V2312
Solution

This error will show up when you try to start the Immersive Explorer, but you are missing one of the prerequisites, DirectX End-User Runtime

You can solve this by manually installing DirectX End-User Runtime.

You can find this pre-requisite also in the documentation, with also the instructions and download link.

https://docs.sw.siemens.com/en-US/doc/209349590/PL20230425446868577.xid2251692/xid2251248
After you have installed DirectX the Immersive Explorer should run just fine.

Notes

KB Article ID# PL8773387

Contents

SummaryDetails

Associated Components

Modeling