Dear Siemens Digital Industries Software Customer,
We are pleased to inform you that Tecnomatix version 2402 Full Product is available for download from Siemens Support Center
You may refer to Tecnomatix_2402_Release_Notes.pdf for details concerning the contents of this release.
Use the Following steps to download:
• Login to the https://support.sw.siemens.com
• If you do not have an account, click Register Now and fill out the information.
• Once on Support Center, if you don't see Tecnomatix under Product Centers , click Manage Product List .
o Scroll down and toggle On the Tecnomatix product .
o Scroll back to the top and click Support Center in the breadcrumb.
• Select Tecnomatix from Product Centers
• Select Downloads
• Select Tecnomatix 2402 under Major Releases tab
• Download the file(s):
• Select Tecnomatix 2402 CAD Translator under Major Releases tab
• Download the file: CAD_Translators_2402.zip
To Install Tecnomatix V2402:
• Extract Tecnomatix_2402_Setups.zip
• Execute (as administrator) 'Setup.exe' in CD2402_Tecnomatix\Setup\64bit
• The default installation folder is C:\Program Files\Tecnomatix_2402
Please note: Starting from Tecnomatix version 2402, we are adopting a new policy of distributing software Release Updates. Instead of providing hotfixes for individual issues, Siemens now publishes monthly Release Updates throughout the first year of the version. These Release Updates incorporate various fixes and improvements for the main release, and each Release Update includes all the content from previous ones. When a new Release Update is available on the Siemens Support Center, upon running Process Simulate the user will be prompted to download and install it.
Sincerely,
Siemens Digital Industries Software