Disabling TC integration on a single workstation.

2024-02-13T16:57:58Z

Summary


Details

How to turn off or disable the Solid Edge Teamcenter Integration on a workstation that does not need access to Teamcenter?

Platforms
  • na windows-1064
Release Versions
  • Solid Edge V224.0
Solution

To turn off the Teamcenter Integration on a Solid Edge client, open Solid Edge without any files. Open and select File and go to Manage then turn off the Teamcenter toggle. The user can toggle it back on if necessary.

To disable the Teamcenter Integration on a workstation is in the Solid Edge PDM Client - Application Launcher. You can find it in the Solid Edge program group labeled "Choose PDM Integration".

Once you have the Solid Edge PDM Client - Application Launcher tool open you will see two options on the Home tab: Solid Edge Data Management and Teamcenter Integration. Select the Solid Edge Data Management option on the workstation that will not be using the Teamcenter integration. That will change the options on the Manage tab in Solid Edge Options so the user will not be able to accidentally enable Teamcenter and consume a SEEC license.

Notes

KB Article ID# PL8772679

Contents

SummaryDetails

Associated Components