OUTPUT CONTACT TRACKING DATA TURN ON = NEED TO BE NOTIFIED

2024-07-12T13:10:23Z

Summary


Details

Problem:

When trying to use NXOpen to access the Zlevel Undercut operation in CAM the operation returns its type as "surface countour" causing a crash in the SurfaceCountourBuilder().

Platforms
  • na windows-1064
Release Versions
  • NX V2306
Solution

Solution:

Zlevel Undercut identifies as a "surface contour", however, a new builder has been created for this operation. You can work around this by using code similar to:

If TypeOf camObject Is CAM.SurfaceContour Then          ' This is a Fixed Axis Surface Contour Operation

        If camObject.GetNameOfType() = "Zlevel Undercut"

           operationType = "Zlevel Undercut"

        Else

            operationType = "Surface Contour"

        End If

Then creating a builder using the correctly identified operationType.

Alternatively, you can also call a new CreateBuilder method on any operation where the builder determines the proper builder to return:

{

For Each operation As NXOpen.CAM.Operation In  setup.CAMOperationCollection()

  operationBuilder = setup.CAMOperationCollection().CreateBuilder(operation)  ' automatically finds the op type and chooses the correct builder to return.

}

Notes

KB Article ID# PL8771500

Contents

SummaryDetails

Associated Components