Solid Edge Reset Emergency Licenses

2024-07-30T16:22:55Z
SETUP

Summary


Details

Once a customer exceeds the maximum number of used emergency licenses, is it possible to reset the count of emergency licenses?

Solution

A customer can download three emergency licenses during any 60-day period.

Once the customer reaches this three license limit, new emergency licenses cannot be generated until the 60-day period has expired. 

It is not possible to reset the number of generated emergency license files, even if the previously generated emergency licenses were not used.

If a customer has exceeded their maximum number of emergency license files and needs another emergency license, the customer can contact PLMS and PLMS can override and generate an additional emergency license file. 

Notes

If you have further inquiries about Solid Edge General Licensing please refer to the FAQs Collection link below:

Solid Edge General Licensing FAQs Collection

KB Article ID# PL8770827

Contents

SummaryDetails

Associated Components

SETUP: LICENSING