Tecnomatix Tecnomatix Controllers for KUKA_KRC, KUKA_KRC_BMW, OLP_TOOL

2024-01-19T06:34:57Z
Process Simulate

Summary


Details

Dear Siemens Digital Industries Software Customer,

We are pleased to inform you that Tecnomatix controllers for "KUKA_KRC, KUKA_KRC_BMW, OLP_TOOL"

are available for download from https://support.sw.siemens.com.

See Tecnomatix_<ControllerName>_changes_log.html for details concerning this update.

Note: This file is located in the 'Robot Controllers Change Logs' folder directly under the 'Tecnomatix <Version> Robot Controllers' folder.

Use the following steps to download:

- Login to https://support.sw.siemens.com

- If you do not have an account, click 'Register Now' and fill out the information.

- Once on Support Center, if you do not see Tecnomatix under 'My Products', click 'Manage Products'.

- Scroll down and toggle On the Tecnomatix product.

- Scroll back to the top and click Support Center in the breadcrumb.

- Select 'Tecnomatix' from 'My Products'

- Select 'Download'

- Select Tecnomatix 16.0, 16.1, 16.1.1, 16.1.2, 17.0, 2206, 2301 or 2307

-Select Tecnomatix 16.0 Robot Controllers, Tecnomatix 16.1 Robot Controllers, Tecnomatix 16.1.1 Robot Controllers, Tecnomatix 16.1.2 Robot Controllers, Tecnomatix 17.0 Robot Controllers, Tecnomatix 2206 Robot Controllers, Tecnomatix 2301 Robot Controllers or Tecnomatix 2307 Robot Controllers

Download the file(s):

Tecnomatix_16.0_KUKA_KRC_64BIT_v6.10.1_18_01_2024.exe

Tecnomatix_16.0_KUKA_KRC_BMW_64BIT_v4.26.1_18_01_2024.exe

Tecnomatix_16.0_OLP_TOOL_64BIT_v16.3.3_18_01_2024.exe

Tecnomatix_16.1_KUKA_KRC_64BIT_v6.10.1_18_01_2024.exe

Tecnomatix_16.1_KUKA_KRC_BMW_64BIT_v4.26.1_18_01_2024.exe

Tecnomatix_16.1_OLP_TOOL_64BIT_v16.3.3_18_01_2024.exe

Tecnomatix_16.1.1_KUKA_KRC_64BIT_v6.10.1_18_01_2024.exe

Tecnomatix_16.1.1_KUKA_KRC_BMW_64BIT_v4.26.1_18_01_2024.exe

Tecnomatix_16.1.1_OLP_TOOL_64BIT_v16.3.3_18_01_2024.exe

Tecnomatix_16.1.2_KUKA_KRC_64BIT_v6.10.1_18_01_2024.exe

Tecnomatix_16.1.2_KUKA_KRC_BMW_64BIT_v4.26.1_18_01_2024.exe

Tecnomatix_16.1.2_OLP_TOOL_64BIT_v16.3.3_18_01_2024.exe

Tecnomatix_17.0_KUKA_KRC_64BIT_v6.10.1_18_01_2024.exe

Tecnomatix_17.0_KUKA_KRC_BMW_64BIT_v4.26.1_18_01_2024.exe

Tecnomatix_17.0_OLP_TOOL_64BIT_v16.3.3_18_01_2024.exe

Tecnomatix_2206_KUKA_KRC_64BIT_v6.10.1_18_01_2024.exe

Tecnomatix_2206_KUKA_KRC_BMW_64BIT_v4.26.1_18_01_2024.exe

Tecnomatix_2206_OLP_TOOL_64BIT_v16.3.3_18_01_2024.exe

Tecnomatix_2301_KUKA_KRC_64BIT_v6.10.1_18_01_2024.exe

Tecnomatix_2301_KUKA_KRC_BMW_64BIT_v4.26.1_18_01_2024.exe

Tecnomatix_2301_OLP_TOOL_64BIT_v16.3.3_18_01_2024.exe

Tecnomatix_2307_KUKA_KRC_64BIT_v6.10.1_18_01_2024.exe

Tecnomatix_2307_KUKA_KRC_BMW_64BIT_v4.26.1_18_01_2024.exe

Tecnomatix_2307_OLP_TOOL_64BIT_v16.3.3_18_01_2024.exe

To Install:

Place Tecnomatix_<TecnomatixVersion>_<ControllerName>_NNBIT_vVV_MM_DD_YYYY.exe into a folder ($Tecnomatix/downloads is suggested, where $Tecnomatix is the full path to the Tecnomatix installation).

Run Tecnomatix_<TecnomatixVersion>_<ControllerName>_NNBIT_vVV_MM_DD_YYYY.exe.

The default installation point is C:\Program Files\Tecnomatix.

If you have any issues with the installation or support of these fixes,

please contact your local GTAC support group.

Sincerely,

Siemens Digital Industries Software

KB Article ID# PL8769784

Contents

SummaryDetails

Associated Components

Process Simulate Off-Line Programming (OLP)