NX What are the two different volumes reported in the Measure Command

2024-01-22T12:27:21Z
NX for Design

Summary


Details

What are the two different volumes reported in the Measure Command?

Platforms
  • na windows-1064
Release Versions
  • NX V2306.6000
Solution

There is a good possibility that the 'Other' option under the Result Filter group has been enabled.  This icon will be highlighted and can be toggled On/Off.  The Measure Preferences can also be reviewed to see if Bounding Box is enabled on the 'Other' tab.



Notes

KB Article ID# PL8769703

Contents

SummaryDetails

Associated Components

Modeling