Tecnomatix Controllers for ESTUN_ERL, SIASUN_SNRC

2024-01-17T05:19:25Z

Summary


Details

Dear Siemens Digital Industries Software Customer,

We are pleased to inform you that Tecnomatix controllers for "ESTUN_ERL, SIASUN_SNRC"

are available for download from https://support.sw.siemens.com.

See Tecnomatix_<ControllerName>_changes_log.html for details concerning this update.

Note: This file is located in the 'Robot Controllers Change Logs' folder directly under the 'Tecnomatix <Version> Robot Controllers' folder.

Use the following steps to download:

- Login to https://support.sw.siemens.com

- If you do not have an account, click 'Register Now' and fill out the information.

- Once on Support Center, if you do not see Tecnomatix under 'My Products', click 'Manage Products'.

- Scroll down and toggle On the Tecnomatix product.

- Scroll back to the top and click Support Center in the breadcrumb.

- Select 'Tecnomatix' from 'My Products'

- Select 'Download'

- Select Tecnomatix 2301 or 2307

-Select Tecnomatix 2301 Robot Controllers or Tecnomatix 2307 Robot Controllers

Download the file(s):

Tecnomatix_2301_ESTUN_ERL_64BIT_v1.2_16_01_2024.exe

Tecnomatix_2301_SIASUN_SNRC_64BIT_v1.1_16_01_2024.exe

Tecnomatix_2307_ESTUN_ERL_64BIT_v1.2_16_01_2024.exe

Tecnomatix_2307_SIASUN_SNRC_64BIT_v1.1_16_01_2024.exe

To Install:

Place Tecnomatix_<TecnomatixVersion>_<ControllerName>_NNBIT_vVV_MM_DD_YYYY.exe into a folder ($Tecnomatix/downloads is suggested, where $Tecnomatix is the full path to the Tecnomatix installation).

Run Tecnomatix_<TecnomatixVersion>_<ControllerName>_NNBIT_vVV_MM_DD_YYYY.exe.

The default installation point is C:\Program Files\Tecnomatix.

If you have any issues with the installation or support of these fixes,

please contact your local GTAC support group.

Sincerely,

Siemens Digital Industries Software

KB Article ID# PL8769183

Contents

SummaryDetails

Associated Components