We have installed Solid Edge 2024 with Solid Edge Data Management (SEDM) on our workstation client and Fast Search 2024 on the server.
Before this installation, the client uses Solid Edge 2023 with Fast Search 2023, without any issue.
After the installation there is the following problem - the client workstation has this error:
At server you can see these options
In Solid Edge 2024 we install the Siemens Connector by default, even if a customer does not have a XaaS configuration. If a customer has a XaaS license (as this end user does) we automatically enable SEDM hard coded.
The message you see here is not an error, it is simply information that the Connector folder should be in the vault definition. Also in this case: it is not relevant if you use the Teamcenter Share application. To remove this message the customer should manually add the Connector location to their vault: