NX About names of parameters displayed in the "Reuse Paste" dialog

2024-01-24T04:12:39Z
NX for Design

Summary


Details

The names of the parameters displayed in the "Reuse Paste" dialog are different from those displayed in the xlsx file.

Names using full brackets are displayed the same in the xlsx file and in the detail parameters.

But some characters may not be displayed for names that use half-width brackets.

Only characters entered within the parentheses are displayed.


Solution

If there are half-width parenthesis in the name, then only the text in the half-width parenthesis will be displayed. When there are half-width parenthesis in the parameter, the format is “expression (description name)”, in this case only the description name is displayed. The parsing of xlsx file currently only supports half-width parentheses.

KB Article ID# PL8768672

Contents

SummaryDetails

Associated Components

Modeling